Hardware Description
General Description
|
A |
24 Vdc power supply terminal block |
|
B |
Modbus address rotary switches |
|
C |
Modbus traffic status LED |
|
D |
Modbus locking pad |
|
E |
ULP status LED |
|
F |
Test button |
|
G |
Mechanical lock |
|
H |
QR code to product information |
|
I |
RJ45 Modbus-SL port |
|
J |
Stacking accessory connection (TRV00217, optional) |
|
K |
2 RJ45 ULP ports |
For information on installation, consult the instruction sheet available on Schneider Electric website: NVE85393.
Mounting
The IFM interface is a DIN rail mounting device. The stacking accessory enables the interconnection of several IFM interfaces without additional wiring.
24 Vdc Power Supply
The IFM interface must always be supplied with 24 Vdc:
-
IFM interfaces stacked to an IFE server are supplied by the IFE server and it is not necessary to supply them separately.
-
If IFM interfaces are stacked without IFE server, only one of the IFM interfaces must be supplied with 24 Vdc.
-
A single IFM interface must be supplied with 24 Vdc.
It is recommended to use an UL listed/UL recognized limited voltage/limited current or a class 2 power supply with a 24 Vdc, 3 A maximum.
Modbus Address Rotary Switches
The IFM interface bears the Modbus address of the IMU to which it is connected. See the ULP System User Guide for more information regarding the IMU.
Define the Modbus address using the two address rotary switches on the front panel of the IFM interface.
The address range is 1 to 99. Do not to use the address 0, because it is reserved for broadcasting commands.
The IFM interface is initially configured with address 99.
Modbus Traffic Status LED
The Modbus traffic status LED provides information about the traffic transmitted or received by the IMU over the Modbus network.
-
When the Modbus address rotary switches are on value 0, the yellow LED is steady ON.
-
When the Modbus address rotary switches are on value anywhere from 1 to 99, the yellow LED is ON during the transmission and reception of messages, OFF otherwise.
Modbus Locking Pad
The Modbus locking pad on the front panel of the IFM interface enables or disables remote control commands to be sent over the Modbus network to the IFM interface itself, and to the other modules of the IMU.
-
If the arrow points to the open padlock (factory setting), remote control commands are enabled.
-
If the arrow points to the closed padlock, remote control commands are disabled.
The only remote control commands that are enabled even if the arrow points to the closed padlock are the Set Absolute Time and Get Current Time commands List of IFM Interface Commands.
Test Button
The test button tests the connection between all the ULP modules connected to the IFM interface.
Pressing the test button launches the connection test for 15 seconds.
During the test, all the ULP modules keep working normally.
ULP Status LED
The yellow ULP status LED describes the mode of the ULP module.
|
ULP status LED |
Mode |
Action |
|---|---|---|
|
Nominal |
None |
|
|
Conflict |
Remove extra ULP module |
|
|
Degraded |
Replace IFM at the next maintenance operation |
|
|
Test |
None |
|
|
Non-critical firmware discrepancy |
Use EcoStruxure Power Commission software to check the firmware and hardware compatibility and follow the recommended actions. |
|
|
Non-critical hardware discrepancy |
||
|
Configuration discrepancy |
Install missing features |
|
|
Critical firmware discrepancy |
Use EcoStruxure Power Commission software to check the firmware and hardware compatibility and follow the recommended actions. |
|
|
Critical hardware discrepancy |
||
|
Stop |
Replace IFM. |
|
|
Power off |
Check power supply |